Write/Read |
About X-Axis Spacing |
Description |
Sets X-axis Point Spacing for the displaytraces measured with segment sweeps on the active channel. |
VB Syntax |
chan.XAxisPointSpacing = value |
Variable |
(Type) - Description |
|
chan |
A Channel (object) |
|
value |
(Enum as naStates) - Choose from: 0 - naOFF - Turns X-axis Point Spacing OFF 1 - naON - Turns X-axis Point Spacing ON |
Return Type |
Enum |
Default |
0 - naOFF |
Examples |
chan.XAxisPointSpacing = naOFF 'Write |
|
xspac = chan.XAxisPointSpacing 'Read |
|
C++ Syntax |
HRESULT get_XAxisPointSpacing (tagNAStates *pState); |
Interface |
IChannel2 |