Specifies settings and fixturing for ground loop de-embedding / embedding.
CALCulate:FSIMulator:GLOop: DEEMBed: | PARameters: | C | L | R | STATe | TYPE EMBed: | PARameters: | C | L | R | STATe | TYPE
|
See Also
Critical Note: CALCulate commands act on the selected measurement. You can select one measurement for each channel using Calc:Par:MNUM or Calc:Par:Select. Learn more.
CALCulate<cnum>:FSIMulator:GLOop:DEEMbed:PARameters:C <value>
Applicable Models: All (Read-Write) Sets and returns the Capacitance, 'C' value for the ground loop de-embedding of the specified channel. Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<value> |
Capacitance value in farads. Choose a value between -1E18 to 1E18 |
Examples |
CALC:FSIM:GLO:DEEM:PAR:C
0.00002 |
Query Syntax |
CALCulate<cnum>:FSIMulator:GLOop:DEEMbed:PARameters:C? |
Return Type |
Numeric |
0 |
|
CALCulate<cnum>:FSIMulator:GLOop:DEEMbed:PARameters:L <value>
Applicable Models: All (Read-Write) Sets and returns the Inductance, 'L' value for the ground loop de-embedding of the specified channel. Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<value> |
Inductance value in henries. Choose a value between -1E18 to 1E18 |
Examples |
CALC:FSIM:GLO:DEEM:PAR:L
0.00002 |
Query Syntax |
CALCulate<cnum>:FSIMulator:GLOop:DEEMbed:PARameters:L? |
Return Type |
Numeric |
0 |
|
CALCulate<cnum>:FSIMulator:GLOop:DEEMbed:PARameters:R <value>
Applicable Models: All (Read-Write) Sets and returns the Resistance, 'R' value for the ground loop de-embedding of the specified channel. Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<value> |
Resistance value in ohms. Choose a value between -1E18 to 1E18 |
Examples |
CALC:FSIM:GLO:DEEM:PAR:R
0.00002 |
Query Syntax |
CALCulate<cnum>:FSIMulator:GLOop:DEEMbed:PARameters:R? |
Return Type |
Numeric |
0 |
|
CALCulate<cnum>:FSIMulator:GLOop:DEEMbed:STATe <bool>
Applicable Models: All (Read-Write) Turns ON or OFF De-embedding for the specified channel. Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<bool> |
Choose from: ON or 1 - Turns De-embedding ON OFF or 0 - Turns De-embedding OFF |
Examples |
CALC:FSIM:GLO:DEEM:STAT
1 |
Query Syntax |
CALCulate<cnum>:FSIMulator:GLOop:DEEMbed:STATe? |
Return Type |
Boolean |
OFF |
|
CALCulate<cnum>:FSIMulator:GLOop:DEEMbed:TYPE <char>
Applicable Models: All (Read-Write) Specifies the circuit model type for ground loop de-embedding. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<char> |
Choose from: USER - Loads s1p file specified using the CALC:FSIM:GLO:DEEM:USER command. RL - Selects Shunt L circuit model. RC - Selects Shunt C circuit mode. |
Examples |
CALC:FSIM:GLO:DEEM:TYPE
RL |
Query Syntax |
CALCulate<cnum>:FSIMulator:GLOop:DEEMbed:TYPE? |
Return Type |
Character |
RL |
|
CALCulate<cnum>:FSIMulator:GLOop:DEEMbed:USER:FILename <filename>
Applicable Models: All (Read-Write) Specifies the filename of the s1p file to load for ground loop de-embedding. Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<filename> |
File name and extension (.s1P) of the de-embedding circuit. Files are stored in the default folder "D:\" To recall from a different folder, specify the full path name. |
Examples |
CALC:FSIM:GLO:DEEM:USER:FIL
'myFile.s1P' |
Query Syntax |
CALCulate<cnum>:FSIMulator:GLOop:DEEMbed:USER:FILename? |
Return Type |
String |
Not Applicable |
|
CALCulate<cnum>:FSIMulator:GLOop:EMBed:PARameters:C <value>
Applicable Models: All (Read-Write) Sets and returns the Capacitance, 'C' value for the ground loop embedding of the specified channel. Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<value> |
Capacitance value in farads. Choose a value between -1E18 to 1E18 |
Examples |
CALC:FSIM:GLO:EMB:PAR:C
0.00002 |
Query Syntax |
CALCulate<cnum>:FSIMulator:GLOop:EMBed:PARameters:C? |
Return Type |
Numeric |
0 |
|
CALCulate<cnum>:FSIMulator:GLOop:EMBed:PARameters:L <value>
Applicable Models: All (Read-Write) Sets and returns the Inductance, 'L' value for the ground loop embedding of the specified channel. Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<value> |
Inductance value in henries. Choose a value between -1E18 to 1E18 |
Examples |
CALC:FSIM:GLO:EMB:PAR:L
0.00002 |
Query Syntax |
CALCulate<cnum>:FSIMulator:GLOop:EMBed:PARameters:L? |
Return Type |
Numeric |
0 |
|
CALCulate<cnum>:FSIMulator:GLOop:EMBed:PARameters:R <value>
Applicable Models: All (Read-Write) Sets and returns the Resistance, 'R' value for the ground loop embedding of the specified channel. Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<value> |
Resistance value in ohms. Choose a value between -1E18 to 1E18 |
Examples |
CALC:FSIM:GLO:EMB:PAR:R
0.00002 |
Query Syntax |
CALCulate<cnum>:FSIMulator:GLOop:EMBed:PARameters:R? |
Return Type |
Numeric |
0 |
|
CALCulate<cnum>:FSIMulator:GLOop:EMBed:STATe <bool>
Applicable Models: All (Read-Write) Turns ON or OFF Embedding for the specified channel. Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<bool> |
Choose from: ON or 1 - Turns Embedding ON OFF or 0 - Turns Embedding OFF |
Examples |
CALC:FSIM:GLO:EMB:STAT
1 |
Query Syntax |
CALCulate<cnum>:FSIMulator:GLOop:EMBed:STATe? |
Return Type |
Boolean |
OFF |
|
CALCulate<cnum>:FSIMulator:GLOop:EMBed:TYPE <char>
Applicable Models: All (Read-Write) Specifies the circuit model type for ground loop embedding. Learn more. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<char> |
Choose from: USER - Loads s1p file specified using the CALC:FSIM:GLO:EMB:USER command. RL - Selects Shunt L circuit model. RC - Selects Shunt C circuit mode. |
Examples |
CALC:FSIM:GLO:EMB:TYPE
RL |
Query Syntax |
CALCulate<cnum>:FSIMulator:GLOop:EMBed:TYPE? |
Return Type |
Character |
RL |
|
CALCulate<cnum>:FSIMulator:GLOop:EMBed:USER:FILename <filename>
Applicable Models: All (Read-Write) Specifies the filename of the s1p file to load for ground loop embedding. Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<filename> |
File name and extension (.s1P) of the embedding circuit. Files are stored in the default folder "D:\" To recall from a different folder, specify the full path name. |
Examples |
CALC:FSIM:GLO:EMB:USER:FIL
'myFile.s1P' |
Query Syntax |
CALCulate<cnum>:FSIMulator:GLOop:EMBed:USER:FILename? |
Return Type |
String |
Not Applicable |
|
CALCulate<cnum>:FSIMulator:GLOop:PORTs <p1>,<p2>,<p3>,<p4>
Applicable Models: All (Read-Write) Specifies the VNA port connections for ground loop embedding/de-embedding. Ground loop ports are typically automatically determined based on the requested measurements, fixturing ports, and calibration ports. However, if it is desired to set them specifically, use this command.
|
|
Parameters |
|
<cnum> |
Channel number of the measurement. |
<p1>,<p2>,<p3>,<p4> |
VNA port number assignment. |
Examples |
CALC:FSIM:GLO:PORT
1,2 |
Query Syntax |
CALCulate<cnum>:FSIMulator:GLOop:PORTs? |
Return Type |
Numeric |
Not Applicable |
|