Calculate and display amplitude modulation or phase modulation per trace. This feature is supported on all standard channels and on all memory traces in a standard channel.
CALCulate:MEASure:DISTortion BACKoff: | [:STATe] SLOPe: | APERture | [:STATe]
|
Click a keyword to view the command details.
See Also
Applicable Models: All (Read-Write) Sets the compression level used in determining the back off calculation. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<num> |
Compression level. |
Examples |
CALC1:MEAS2:DIST:BACK:COMP 1 dB calculate2:measure2:distortion:backoff:compression 1 dB |
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:DISTortion:BACKoff:COMPression? |
Return Type |
Numeric |
1 dB |
|
Applicable Models: All (Read-Write) Enables/disables compression level back off function specified using the CALCulate:MEASure:DISTortion:BACKoff:COMPression command. When enabled, the x-axis changes to display the back off from the compression point. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<bool> |
Compression level back off state. Choose from: 0 - Compression level back off state OFF 1 - Compression level back off state ON |
Examples |
CALC:MEAS2:CORR ON calculate:measure2:correction:state off |
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:DISTortion:BACKoff[:STATe]? |
Return Type |
Boolean |
OFF |
|
CALCulate<cnum>:MEASure<mnum>:DISTortion:MODE <char>
Applicable Models: All (Read-Write) Displays phase or amplitude distortion. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<char> |
Choose from:
|
Examples |
CALC:MEAS:DIST:MODE
AMAM |
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:DISTortion:MODE? |
Return Type |
Character |
OFF |
|
Applicable Models: All (Read-Write) Sets the aperture value over which the phase or gain slope will be calculated. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<num> |
Aperture value. |
Examples |
CALC1:MEAS2:DIST:SLOP:APER 1 dB calculate2:measure2:distortion:slope:aperture 1 dB |
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:DISTortion:SLOPe:APERture? |
Return Type |
Numeric |
1 dB |
|
Applicable Models: All (Read-Write) Enables/disables phase slope (AMPM) or gain slope (AMAM) over the slope aperture to be displayed. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<bool> |
Compression level back off state. Choose from: 0 - Phase or gain slope over aperture state OFF 1 - Phase or gain slope over aperture state ON |
Examples |
CALC:MEAS2:DIST:SLOP ON calculate:measure2:distortion:slope:state off |
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:DISTortion:SLOPe[:STATe]? |
Return Type |
Boolean |
OFF |
|