These commands are for setting up bandwidth tests.
CALCulate:MEASure:BLIMit BWIDth DISPlay | MARKer | STATe REPort | DATA? |
Click a keyword to view the command details.
See Also
Applicable Models: All (Read-Write) Sets bandwidth threshold value (attenuation from the peak) of the bandwidth test. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<value> |
Bandwidth N dB points |
Examples |
CALC:MEAS:BLIM:BWID:THR
5 |
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:BLIMit:BWIDth:THReshold? |
Return Type |
Numeric |
3 |
|
Applicable Models: All (Read-Write) Turns ON/OFF the bandwidth value display of the bandwidth test, for the active trace of selected channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<bool> |
ON or 1 - Turns limit
testing ON. |
Examples |
CALC:MEAS:BLIM:DISP:MARK:STAT
ON |
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:BLIMit:DISPLay:BWIDth:STATe? |
Return Type |
Boolean |
OFF |
|
Applicable Models: All (Read-only) Get the bandwidth limit test results, for the active trace of selected channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<bool> |
Boolean
|
Examples |
CALC:MEAS:BLIM:FAIL? |
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:BLIMit:FAIL? |
Return Type |
Boolean |
Not Applicable |
|
Applicable Models: All (Read-Write) Sets/gets the upper limit value of the bandwidth test, for the selected channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<max> |
Maximum bandwidth |
Examples |
CALC:MEAS:BLIM:MAX
1E6 |
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:BLIMit:MAXimum? |
Return Type |
Numeric |
300000 |
|
Applicable Models: All (Read-Write) Sets or returns the lower limit value of the bandwidth test, for the selected channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<min> |
Minimum bandwidth |
Examples |
CALC:MEAS:BLIM:MIN
1E6 |
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:BLIMit:MINimum? |
Return Type |
Numeric |
10000 |
|
Applicable Models: All (Read-only) Read the bandwidth value of the bandwidth test, for the active trace of selected channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
Examples |
CALC:MEAS:BLIM:REP:DATA? |
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:BLIMit:REPort:DATA? |
Return Type |
Numeric |
OFF |
|
Applicable Models: All (Read-Write) Turns ON/OFF the bandwidth test function, for the active trace of selected channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<bool> |
ON or 1
- Turns limit testing ON. |
Examples |
CALC:MEAS:LIM:STAT
ON |
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:BLIMit:DIPLay:MARKer:STATe? |
Return Type |
Boolean |
OFF |
|