Controls the display of X-axis for various measurements.
CALCulate:MEASure:X | DOMain | FIXed | VALue | UNIT? |
Click a keyword to view the command details.
See Also
Applicable Models: All (Write-Read) Sets the X-axis of the selected measurement. This command does not change the default setting for new traces. |
|
Parameters |
|
<ch> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<string> |
String - (Not case-sensitive) For all channels EXCEPT DIQ, choose from the following: "Default" - The default X-axis setting for the selected measurement. For Application measurements, the X-Axis domain is set with specific commands. "AO1" - Internal DC source #1 "AO2" - Internal DC source #2 Note: For DIQ channels, see CALC:MEAS:X:AXIS:DOMain
For Modulation Distortion Channels (MOD), choose from: "SA Frequency" - SA display showing the SA frequency settings. "Power In" - Displays input power sweep. "Power Out" - Displays output power sweep. "Measured Carrin" - Measured input band power. "Measured CarrOut" - Measured output band power.
For Modulation Distortion Converters Channels (MODX), choose from: "SA Freq In" - SA display showing mixer input range. "SA Freq Out" - SA display showing mixer output range. "Power In" - Displays input power sweep. "Power Out" - Displays output power sweep. "Measured Carrin" - Measured input band power. "Measured CarrOut" - Measured output band power.
|
Examples |
CALC:MEAS2:X:AXIS 'Default' calculate:measure2:x:axis "AO1" |
Query Syntax |
CALCulate<ch>:MEASure<mnum>:X:AXIS? |
Return Type |
String |
"Default" |
|
Applicable Models: All (Write-Read) Sets and returns the X-Axis domain of the selected DIQ measurement. |
|||||||||||||
Parameters |
|
||||||||||||
<ch> |
Channel number of the measurement (optional). |
||||||||||||
<mnum> |
Measurement number for each measurement. |
||||||||||||
|
|
||||||||||||
Example |
1. CALC:MEAS2:X:AXIS:DOM "Power" 2. CALC:MEAS2:X:AXIS "Port 1" |
||||||||||||
Query Syntax |
CALCulate<ch>:MEASure<mnum>:X:AXIS:DOMain? |
||||||||||||
Return Type |
String |
||||||||||||
CALC:MEAS:X:AXIS:DOMain: "Frequency" CALC:MEAS:X:AXIS: "F1" |
|||||||||||||
Applicable Models: All with Option S93070xB or S9x070B (Write-Read) Sets the X-axis fixed parameter for a power sweep measurement in a Modulation Distortion channel. |
|
Parameters |
|
<ch> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<string> |
String - (Not case-sensitive) For Modulation Distortion Channels (MOD), choose from: "SA Frequency" - SA display showing the SA frequency settings.
For Modulation Distortion Converters Channels (MODX), choose from: "SA Freq In" - SA display showing mixer input range. "SA Freq Out" - SA display showing mixer output range.
|
Examples |
CALC:MEAS2:X:AXIS:FIX:PAR "SA Frequency" calculate:measure2:x:axis:fixed:parameter "SA Freq In" |
Query Syntax |
CALCulate<ch>:MEASure<mnum>:X:AXIS:FIXed:PARameter? |
Return Type |
String |
"" |
|
Applicable Models: All with Option S93070xB or S9x070B (Write-Read) Sets the X-axis fixed parameter spectrum analyzer frequency value for a power sweep measurement in a Modulation Distortion channel. |
|
Parameters |
|
<ch> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<num> |
Fixed parameter value. |
Examples |
CALC:MEAS2:X:AXIS:FIX:PAR:VAL 1.5e9 calculate:measure2:x:axis:fixed:parameter:value 1.5e9 |
Query Syntax |
CALCulate<ch>:MEASure<mnum>:X:AXIS:FIXed:PARameter:VALue? |
Return Type |
Numeric |
Not Applicable |
|
Applicable Models: All (Read-only) Returns the current units of the X-axis (FREQuency | POWer | PHASe | DC | POINts | DEFault). This command can be used for all Measurement Classes. |
|
Parameters |
|
<ch> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
Examples |
CALC:MEAS2:X:AXIS:UNIT? |
Return Type |
Enumeration |
FREQuency |
|
Applicable Models: All (Read-only) Returns the stimulus values for the selected measurement in the current units. This command can be used for all Measurement Classes. Note: To avoid frequency rounding errors, specify FORM:DATA <Real,64> or <ASCii, 0> |
|
Parameters |
|
<ch> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
Examples |
1.
Calc:MEAS2:Par:Sel "MyGCATrace" |
Return Type |
Depends on FORM:DATA command |
Not applicable |
|