Controls the display of Y-axis for various measurements.
CALCulate:MEASure:Y AXIS | UNIT? |
Click a keyword to view the command details.
See Also
Applicable Models: All (Read-only) Returns the current units of the Y-axis (HZ | SECond | MINute | HOUR | DAY | DB | DBM | DBMV | WATTs | FARad | HENRy | OHM | MHO | SIEMen | VOLT | DEGRee | RADians | METer | DPHZ | UNIT | NONe | TNORmalized | NTEMperature | KELVin|CENTigrade | FAHRenheit | FEET | INCH | DBMAAMPere | VOLTAge | DBUV | PERCentage | DMVRoothz | DUVRoothz | DMARoothz | WPHZ | VROothz | AROothz | DBC | DVPerhz | DCPerhz | DBPerhz | HZPerhz | PRHz | VPHz | DBV|DEFault). This command can be used for all Measurement Classes. |
|
Parameters |
|
<ch> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
Examples |
CALC:MEAS2:Y:AXIS:UNIT? |
Return Type |
Enumeration |
FREQuency |
|
Applicable Models: All (Read-only) Returns the Y-axis values for the selected measurement in the current units. This command can be used for all Measurement Classes. |
|
Parameters |
|
<ch> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
Examples |
CALC:MEAS2:Y? |
Return Type |
Array of data |
Not applicable |
|