This command is Superseded by the CALCulate:MEASure:MIXer:XAXis command.
CALCulate<ch>:MIXer:XAXis <char>
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA (Read-Write) Sets or returns the swept parameter to display on the X-axis for the selected FCA and GCX measurement. Critical Note: CALCulate commands act on the selected measurement. You can select one measurement for each channel using Calc:Par:MNUM or Calc:Par:Select. Learn more. |
|
Parameters |
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
<char> |
Parameter to display on the X-axis. Choose from: INPUT - Input frequency span OUTPUT - Output frequency span LO_1 - First LO frequency span LO_2 - Second LO frequency span |
Examples |
CALC:MIX:XAX
INPUT See an example that creates, selects, and calibrates an SMC and VMC measurement using SCPI. |
Query Syntax |
CALCulate<ch>:MIXer:XAXis? |
Return Type |
Character |
OUTPUT |
|