Controls the E5092A Configurable Multiport Test Set.
CONTrol:MULTiplexer: OUTPut PORT
|
Click on a keyword to view the command details.
See Also
Applicable Models: N522xB, N523xB, N524xB, E5080B, M980xA (Read-Write) Sets or returns the output port data for specified group with id of the E5092A multiport test set. Notes:
|
|||||||||||||||||||
Parameters |
|
||||||||||||||||||
<id> |
Id of the external test set either 1 or 2. If unspecified, Id is assumed to be 1. |
||||||||||||||||||
<grp> |
A | B | C | D |
||||||||||||||||||
<num> |
An integer specifying the decimal value of the control line. Values are obtained by adding weights from the following table that correspond to individual lines. The output port data range is between 0 to 255 (0=All lines are turned OFF and 255 all lines are turned ON).
|
||||||||||||||||||
Examples |
CONT:MULT1:STAT OFF CONT:MULT1:OUTP:B 8 ' immediately output 8 from control line B. |
||||||||||||||||||
Query Syntax |
CONTrol:MULTiplexer<id>:OUTPut:<grp>[:DATa]? |
||||||||||||||||||
Return Type |
Numeric |
||||||||||||||||||
0 |
|||||||||||||||||||
Applicable Models: N522xB, N523xB, N524xB, E5080B, M980xA (Read-Write) Sets or returns the output voltage for specified group with id of the E5092A multiport test set. Notes: |
|
Parameters |
|
<id> |
Id of the external test set either 1 or 2. If unspecified, Id is assumed to be 1. |
<grp> |
A | B | C | D |
<volt> |
Output voltage range for <grp> is between 0 to 5.2V and resolution is 10mV. |
Examples |
CONT:MULT1:STAT OFF CONT:MULT1:OUTP:B:VOLT 4.2 ' immediately set control line B voltage to 4.2 volt. |
Query Syntax |
CONTrol:MULTiplexer<id>:OUTPut:<grp>:VOLtage[:DATa]? |
Return Type |
Numeric |
0 V |
|
Applicable Models: N522xB, N523xB, N524xB, E5080B, M980xA (Write-Only) Sets the multiport test set port. If this command creates a conflict with an existing port, the VNA will resolve the conflict. Notes: |
|
Parameters |
|
<id> |
Id of the external test set. If unspecified, Id is assumed to be 1. Must be previously set by the SENSe:MULT:TYPE command. |
<pnum> |
The VNA connection port number (1 to 4). If the E5092A’s configuration is E5092_28, this parameter specifies the individual switch number (1 to 4: SP4T switches, 5 to 10: SPDT switches). |
<string> |
The label of the E5092A’s measurement port. If the E5092A’s configuration is E5092_28, this parameter specifies the connection of the individual switch. Refer to the table of SENS:MULT:PORT:SEL. |
Examples |
CONT:MULT1:STAT OFF CONT:MULT1:TYP 'E5092_22' CONT:MULT1:PORT1:SEL 'A2' ' set E5092A to 22-port config and immediately connect port1 to 'A2'. |
Return Type |
String |
Not Applicable |
|