When you use the E5080B/81A, you can control the Interface control through the VNA firmware.
SENSe:CONTrol: | [:STATe] | :DWELl | :HANDler | [:DATA] | :DIO | [:STATE] | :VIO | :LEVel | :IOTYpe | :PIO | :TYPE | :LEVel | :RFFE | :CLOCk | :CSEQuence | :TYPE | :BCOunt | :ADDRess | :COUNt | :MACRo | [:STATe] | :COMMand | :FILE | :PATH |
Click on a keyword to view the command details.
Applicable Models: E5080B, E5081A (Read-Write) Sets and read the state of interface control for all channels. Channel number is ignored. |
|
Parameters |
|
<cnum> |
Channel number. |
<bool> |
Module control state. Choose from: O or OFF - Interface control port signals won't be sent. 1 or ON - Interface control port signals will be sent. |
Examples |
SENS:CONT |
Query Syntax |
:SENSe<cnum>:CONTrol:[:STATe]? |
Return Type |
Boolean |
Default |
OFF or 0 |
Preset |
0 |
Save or Recall |
Yes |
Applicable Models: E5080B, E5081A (Read-Write) Sets and read the delay time between the time all interface control port signals and all commands sent and the one measurements start. Set independently per channel and for forward and reverse sweep. Not set per IO type. |
|
Parameters |
|
<cnum> |
Channel number. |
<char> |
Character - when to send remote commands. Choose from: AFTer - After the channel sweep ends. BEFore - Before the channel sweep starts. |
<num> |
Wait time in milliseconds. Any positive integer is allowed. |
Examples |
SENS:CONT:DWEL
BEF 10 |
Query Syntax |
:SENSe<cnum>:CONTrol:DWELl? <char> |
Return Type |
Character |
Default |
0 |
Preset |
0 |
Save or Recall |
Yes |
Applicable Models: E5080B, E5081A (Read-Write) Sends values to the respective Handler I/O port (A-D). Although ports C and D are normally bidirectional, ONLY Output mode is allowed using the Interface Control feature. It cannot read from these, or any other ports. |
|
Parameters |
|
<cnum> |
Channel number. |
<grp> |
Port identifier to set bits for. Choose from: A, B, C and D. |
<char> |
Character - when to send remote commands. Choose from: AFTer - After the channel sweep ends. BEFore - Before the channel sweep starts. |
<num> |
The number of the data bits to set. The range of the value is determined as follows. Port A: 0 - 255 Port B: 0 - 255 Port C: 0 - 15 Port D: 0 - 15 |
Examples |
SENS:CONT:HAND:B
AFT, 255 |
Query Syntax |
:SENSe<cnum>:CONTrol:HANDler:<grp>[:DATA]? <char> |
Return Type |
Numeric |
Default |
0 |
Preset |
0 |
Save or Recall |
Yes |
Applicable Models: E5080B, E5081A (Read-Write) Set and read the control function state for each channel. If ON, Handler I/O port signals will be sent before the beginning of the sweep or after the end of the sweep. If OFF, these signals will not be changed. |
|
Parameters |
|
<cnum> |
Channel number. |
<char> |
Character - when to send remote commands. Choose from: AFTer - After the channel sweep ends. BEFore - Before the channel sweep starts. |
<bool> |
Choose from: ON (1) - Handler I/O port signals will be sent. OFF (0) - Handler I/O port signals won't be sent. |
Examples |
SENS:CONT:HAND
AFT, ON |
Query Syntax |
:SENSe<cnum>:CONTrol:HANDler[:STATe]? <char> |
Return Type |
Boolean |
Default |
1 |
Preset |
1 |
Save or Recall |
Yes |
Applicable Models: E5080B, E5081A (Read-Write) Set and read the control function state for each channel. If ON, DUT control signals will be sent before the beginning of the sweep or after the end of the sweep. If OFF, then DUT signals will not be changed. |
|
Parameters |
|
<cnum> |
Channel number. |
<id> |
DIO number, 1 or 2 |
<char> |
Character - when to send remote commands. Choose from: AFTer - After the channel sweep ends. BEFore - Before the channel sweep starts. |
<bool> |
Function enable or disable control. Choose from: ON or OFF |
Examples |
SENS:CONT:DIO1
AFT, ON |
Query Syntax |
:SENSe<cnum>:CONTrol:DIO<id>[:STATe]? <char> |
Return Type |
Boolean (1= ON, 0= OFF) |
Default |
OFF |
Applicable Models: E5080B, E5081A (Read-Write) Set and read the VIO function state for each channel. If ON, then VIO's voltage is set to the value which is determined by SENSe:CONTrol:DIO:LEVel before the beginning of the sweep or after the end of he sweep. If OFF, the VIO's voltage is disabled. |
|
Parameters |
|
<cnum> |
Channel number. |
<id> |
DIO number, 1 or 2 |
<char> |
Character - when to send remote commands. Choose from: AFTer - After the channel sweep ends. BEFore - Before the channel sweep starts. |
<bool> |
Function enable or disable control. Choose from: ON or OFF |
Examples |
SENS:CONT:DIO1:VIO
AFT, OFF |
Query Syntax |
:SENSe<cnum>:CONTrol:DIO<id>:VIO[:STATe]? <char> |
Return Type |
Boolean (1= ON, 0= OFF) |
Default |
ON |
Applicable Models: E5080B, E5081A (Read-Write) Specifies IO level of the DUT Control DIO1 or DIO2's 8-bit IO. The value of AFTer is overwritten by the one of BEFore and vice versa due to set the same value to both AFTer and BEFore. |
|
Parameters |
|
<cnum> |
Channel number. |
<id> |
DIO number, 1 or 2 |
<char> |
Character - when to send remote commands. Choose from: AFTer - After the channel sweep ends. BEFore - Before the channel sweep starts. |
<num> |
IO level in volt. Value range, 0.9 to 3.5, step 0.05. |
Examples |
SENS:CONT:DIO1:VIO
AFT, OFF |
Query Syntax |
:SENSe<cnum>:CONTrol:DIO<id>:LEVel? <char> |
Return Type |
Numeric |
Default |
1.2 |
Note: The default value definition comes from MIPI RFFE standard. Referring to the VIO Supply Pin Requirements, 1.2V is the minimum typical voltage value of the definition.
Applicable Models: E5080B, E5081A (Write only) Specifies parameter set of DUT Control function for each channel. And, fetch E5080B Hardware status values (PIO input state, RFFE read command results) and stores the values in Firmware variables. If executed, the DUT signals will be sent immediately. It doesn't matter if Enable DUT Control is ON or OFF. |
|
Parameters |
|
<cnum> |
Channel number. |
<id> |
DIO number, 1 or 2 |
<char> |
Character - when to send remote commands. Choose from: AFTer - After the channel sweep ends. BEFore - Before the channel sweep starts. |
Examples |
SENS:CONT:DIO1:IMM BEF |
Query Syntax |
Not applicable |
Default |
Not applicable |
Applicable Models: E5080B, E5081A (Read-Write) Specifies IO function type of the 8-bit IO pin, for each IO group. IO group1 is IO pin 1 and 2, group2 is pin 3 and 4, group3 is pin 5 and 6, group4 is pin 7 and 8. |
|
Parameters |
|
<cnum> |
Channel number. |
<id> |
DIO number, 1 or 2 |
<iogroup> |
IO group number. Value range, 1 to 4. |
<char> |
Character - when to send remote commands. Choose from: AFTer - After the channel sweep ends. BEFore - Before the channel sweep starts. |
<enum> |
Set the IO function for the IO group. Choose from: PARallel or RFFE |
Examples |
SENS:CONT:DIO1:IOTY
AFT, RFFE |
Query Syntax |
:SENSe<cnum>:CONTrol:DIO<id>:IOTYpe<iogroup>? <char> |
Return Type |
Character |
Default |
PARallel |
Applicable Models: E5080B, E5081A (Read-Write) Set or read the signal direction type of Parallel IO, for each IO pin.. This setting is valid when the IO pin function is selected as parallel IO. |
|
Parameters |
|
<cnum> |
Channel number. |
<id> |
DIO number, 1 or 2 |
<iopin> |
IO pin number. |
<char> |
Character - when to send remote commands. Choose from: AFTer - After the channel sweep ends. BEFore - Before the channel sweep starts. |
<enum> |
IO direction. Choose from: IN or OUT |
Examples |
SENS:CONT:DIO1:PIO:TYPE
AFT, IN |
Query Syntax |
:SENSe<cnum>:CONTrol:DIO<id>:PIO<iopin>:TYPE? <char> |
Return Type |
Character |
Default |
OUT |
Applicable Models: E5080B, E5081A (Read-Write) Set or read the signal level of IO pin, high or low. This setting is valid when the IO pin function is selected as parallel IO. If the IO type is IN, this command shall be a read-only command. Write command will cause error. |
|
Parameters |
|
<cnum> |
Channel number. |
<id> |
DIO number, 1 or 2 |
<iopin> |
IO pin number. |
<char> |
Character - when to send remote commands. Choose from: AFTer - After the channel sweep ends. BEFore - Before the channel sweep starts. |
<enum> |
Signal level. Choose from: HIGH or LOW |
Examples |
SENS:CONT:DIO1:PIO:LEV
AFT, HIGH |
Query Syntax |
:SENSe<cnum>:CONTrol:DIO<id>:PIO<iopin>:LEVel? <char> |
Return Type |
Character |
Default |
LOW |
Applicable Models: E5080B, E5081A (Read-Write) Set or read the RFFE clock rate. |
|
Parameters |
|
<cnum> |
Channel number. |
<id> |
DIO number, 1 or 2 |
<char> |
Character - when to send remote commands. Choose from: AFTer - After the channel sweep ends. BEFore - Before the channel sweep starts. |
<num> |
Clock rate in Hz. Value range, 25kHz to 25000kHz. Possible values are (50000/n) kHz, with integer n, 2000 to 2. |
Examples |
SENS:CONT:DIO1:RFFE:CLOC
AFT, 25000 |
Query Syntax |
:SENSe<cnum>:CONTrol:DIO<id>:RFFE:CLOCk? <char> |
Return Type |
Numeric |
Default |
50000 |
Note: The default value is the minimum integer value of clock rate, which meets the RFFE standard frequency range.
Applicable Models: E5080B, E5081A (Read-Write) Set or read the secondary address (“SA” in GUI) for the specified command sequence. |
|
Parameters |
|
<cnum> |
Channel number. |
<id> |
DIO number, 1 or 2 |
<rffech> |
RFFE channel number. 1 to 4. |
<csnum> |
RFFE command sequence number. 1 to 16. |
<char> |
Character - when to send remote commands. Choose from: AFTer - After the channel sweep ends. BEFore - Before the channel sweep starts. |
<num> |
DUT RFFE secondary address. 0 to 15. |
Examples |
SENS:CONT:DIO1:RFFE:CSEQ:SADD
AFT, 2 |
Query Syntax |
:SENSe<cnum>:CONTrol:DIO<id>:RFFE<rffech>:CSEQuence<csnum>:SADDress? <char> |
Return Type |
Numeric |
Default |
0 |
Applicable Models: E5080B, E5081A (Read-Write) Set or read the command sequence type for the specified command sequence. |
|
Parameters |
|
<cnum> |
Channel number. |
<id> |
DIO number, 1 or 2 |
<rffech> |
RFFE channel number. 1 to 4. |
<csnum> |
RFFE command sequence number. 1 to 16. |
<char> |
Character - when to send remote commands. Choose from: AFTer - After the channel sweep ends. BEFore - Before the channel sweep starts. |
<enum> |
RFFE command sequence type. Choose from: R0WRite: Register 0 Write RREad: Register Read RWRite: Register Write ERRead: Extended Register Read ERWRite : Extended Register Write |
Examples |
SENS:CONT:DIO1:RFFE:CSEQ:TYPE
AFT, R0WR |
Query Syntax |
:SENSe<cnum>:CONTrol:DIO<id>:RFFE<rffech>:CSEQuence<csnum>:TYPE? <char> |
Return Type |
Character |
Default |
RREad |
Applicable Models: E5080B, E5081A (Read-Write) Set and read the byte count for the specified command sequence. |
|||||||
Parameters |
|
||||||
<cnum> |
Channel number. |
||||||
<id> |
DIO number, 1 or 2 |
||||||
<rffech> |
RFFE channel number. 1 to 4. |
||||||
<csnum> |
RFFE command sequence number. 1 to 16. |
||||||
<char> |
Character - when to send remote commands. Choose from: AFTer - After the channel sweep ends. BEFore - Before the channel sweep starts. |
||||||
<num> |
Byte Count value. Integer value. The value range is coupled with command sequence type setting.
|
||||||
Examples |
SENS:CONT:DIO1:RFFE:CSEQ:BCO
AFT, 4 |
||||||
Query Syntax |
:SENSe<cnum>:CONTrol:DIO<id>:RFFE<rffech>:CSEQuence<csnum>:BCOunt? <char> |
||||||
Return Type |
Numeric |
||||||
Default |
1 |
||||||
Applicable Models: E5080B, E5081A (Read-Write) Set and read the address value for the specified command sequence. |
|||||||||
Parameters |
|
||||||||
<cnum> |
Channel number. |
||||||||
<id> |
DIO number, 1 or 2 |
||||||||
<rffech> |
RFFE channel number. 1 to 4. |
||||||||
<csnum> |
RFFE command sequence number. 1 to 16. |
||||||||
<char> |
Character - when to send remote commands. Choose from: AFTer - After the channel sweep ends. BEFore - Before the channel sweep starts. |
||||||||
<num> |
Address value. Integer value. The value range is coupled with command sequence type setting.
|
||||||||
Examples |
SENS:CONT:DIO1:RFFE:CSEQ:ADDR
AFT, 4 |
||||||||
Query Syntax |
:SENSe<cnum>:CONTrol:DIO<id>:RFFE<rffech>:CSEQuence<csnum>:ADDRess? <char> |
||||||||
Return Type |
Numeric |
||||||||
Default |
0 |
||||||||
Applicable Models: E5080B, E5081A (Read-Write) Set and read the data values for the specified command sequence. This command works if the command sequence type is “Register 0 Write” or “Register Write” or “Extended Register Write”. If the command sequence type is “Register Read” or ”Extended Register Read”, this command will cause error. |
|
Parameters |
|
<cnum> |
Channel number. |
<id> |
DIO number, 1 or 2 |
<rffech> |
RFFE channel number. 1 to 4. |
<csnum> |
RFFE command sequence number. 1 to 16. |
<char> |
Character - when to send remote commands. Choose from: AFTer - After the channel sweep ends. BEFore - Before the channel sweep starts. |
<data> |
Comma separated list of data values. The value length is coupled with byte count setting. If data list length does not match with byte count setting, write command will cause error. |
Examples |
SENS:CONT:DIO1:RFFE:CSEQ:WRIT:DATA
AFT, 10 |
Query Syntax |
:SENSe<cnum>:CONTrol:DIO<id>:RFFE<rffech>:CSEQuence<csnum>[:WRITe]:DATA? <char> |
Return Type |
Comma separated numeric values |
Default |
0 |
Applicable Models: E5080B, E5081A (Read only) Read the data and parity value pairs from DUT for the specified command sequence. |
|
Parameters |
|
<cnum> |
Channel number. |
<id> |
DIO number, 1 or 2 |
<rffech> |
RFFE channel number. 1 to 4. |
<csnum> |
RFFE command sequence number. 1 to 16. |
<char> |
Character - when to send remote commands. Choose from: AFTer - After the channel sweep ends. BEFore - Before the channel sweep starts. |
Examples |
SENS:CONT:DIO1:RFFE:CSEQ:READ:DATA?
AFT |
Query Syntax |
:SENSe<cnum>:CONTrol:DIO<id>:RFFE<rffech>:CSEQuence<csnum>:READ:DATA? <char> |
Return Type |
Comma separated numeric values, list of data and parity pairs. Ex. Byte count is 3 case, return values are below: [data#1],[parity#1],[data#2],[parity#2],[data#3],[parity#3] |
Default |
Not applicable |
Applicable Models: E5080B, E5081A (Read-Write) Set and read the RFFE Command Sequence count. If user set the larger value than previously set, new RFFE Command Sequences will be added with default parameter value. |
|
Parameters |
|
<cnum> |
Channel number. |
<id> |
DIO number |
<rffech> |
RFFE channel number. 1 to 4. |
<char> |
Character - when to send remote commands. Choose from: AFTer - After the channel sweep ends. BEFore - Before the channel sweep starts. |
Examples |
SENS:CONT:DIO1:RFFE:CSEQ:COUN
AFT |
Query Syntax |
:SENSe<cnum>:CONTrol:DIO<id>:RFFE<rffech>:CSEQuence:COUNt? <char> |
Return Type |
Numeric |
Default |
0 |
Applicable Models: E5080B, E5081A, N522xB, N523xB, N524xB (Read-Write) Enables or disables software interface controls. |
|
Parameters |
|
<cnum> |
Channel number. |
<char> |
Character - when to send remote commands. Choose from: AFTer - After the channel sweep ends. BEFore - Before the channel sweep starts. |
<bool> |
ON or 1 - Turns software interface control ON. OFF or 0 - Turns software interface control OFF. |
Examples |
SENS:CONT:MACR
AFT, ON |
Query Syntax |
:SENSe<cnum>:CONTrol:MACRo[:STATe]? <char> |
Return Type |
Boolean |
Default |
OFF |
Applicable Models: E5080B, E5081A, N522xB, N523xB, N524xB (Read-Write) Set and read SCPI commands with target GPIB addresses (numbers) or VISA addresses. The specified SCPI commands are sent to the target instruments before the first trace on the channel begins sweeping. It is the end user’s responsibility to use this command. |
|
Parameters |
|
<cnum> |
Channel number. |
<char> |
Character - when to send remote commands. Choose from: AFTer - After the channel sweep ends. BEFore - Before the channel sweep starts. |
<cmdList> |
The string of “\n” separates a pair of GPIB/VISA addresses and SCPI commands, and the string of “ ” separates GPIB/VISA address and SCPI in the following format; “address1 command1\naddress2 command2\n …” |
Examples |
SENS:CONT:MACR:COMM
AFT |
Query Syntax |
:SENSe<cnum>:CONTrol:MACRo:COMMand? <char> |
Return Type |
String of comma-separated GPIB/VISA addresses and SCPI commands |
Default |
" " |
Applicable Models: E5080B, E5081A, N522xB, N523xB, N524xB (Read-Write) Set and read a file path to a macro. The macro is executed before the first trace on the channel begins sweeping. It is the end user’s responsibility to use this command. It’s needed to check the check box of “Enable Drive Access” in the SCPI dialog to execute the actual macro file. |
|
Parameters |
|
<cnum> |
Channel number. |
<char> |
Character - when to send remote commands. Choose from: AFTer - After the channel sweep ends. BEFore - Before the channel sweep starts. |
<path> |
Command line strings |
Examples |
SENS:CONT:MACR:FILE:PATH
AFT, "cscript
D:\temp\test.vbs" |
Query Syntax |
:SENSe<cnum>:CONTrol:MACRo:FILE:PATH? <char> |
Return Type |
String |
Default |
" " |
Applicable Models: E5080B, E5081A, N522xB, N523xB, N524xB (Read-Write) Set and read arguments for a macro. The macro is executed before the first trace on the channel begins sweeping. It is the end user’s responsibility to use this command. It’s needed to check the check box of “Enable Drive Access” in the SCPI dialog to execute the actual macro file. |
|
Parameters |
|
<cnum> |
Channel number. |
<char> |
Character - when to send remote commands. Choose from: AFTer - After the channel sweep ends. BEFore - Before the channel sweep starts. |
<arg> |
Arguments for a macro |
Examples |
SENS:CONT:MACR:FILE:ARG
AFT, "localhost"
|
Query Syntax |
:SENSe<cnum>:CONTrol:MACRo:FILE:ARGuments? <char> |
Return Type |
String |
Default |
" " |