Click on a keyword to view the command details.
See Also
This command is not necessary, and its use is not recommended. Setting the sweep mode to NONE does not improve the quality of the measurement. Applicable Models: All (Read-Write) Sets the sweep mode as Chopped or Alternate. |
|
Parameters |
|
<cnum> |
Any existing channel number; if unspecified, value is set to 1. |
<ALL | NONE> |
ALL - Sweep mode set to Chopped - reflection and transmission measured on the same sweep. NONE - Sweep mode set to Alternate - reflection and transmission measured on separate sweeps. Increases sweep time |
Examples |
SENS:COUP
ALL |
Query Syntax |
SENSe<cnum>:COUPle? |
Return Type |
Character |
ALL |
|
Applicable Models: All (Read-Write) Turns ON and OFF Time Domain Trace Coupling. All of the measurements in the specified channel are coupled.
Learn more about Time Domain Trace Coupling. |
|
Parameters |
|
<cnum> |
Any existing channel number; if unspecified, value is set to 1. |
<bool> |
ON (or 1) - Turns ON Time Domain Trace Coupling. OFF (or 0) - Turns OFF Time Domain Trace Coupling. |
Examples |
SENS:COUP:PAR
0 |
Query Syntax |
SENSe<cnum>:COUPle:PARameter[:STATe]? |
Return Type |
Boolean |
ON (or 1) |
|