Controls the connection between the VNA and the Vector Signal Analyzer (89600 VSA) Application.
SENSe:VSA CONNect | [:STATe] DATA | MOD | PIN1 | [:STATe] | PINWav | [:STATE] | POU2 | [:STATe] | STReam | [:STATe] DTRigger | [:STATe] FREQuency | CENTer IF | OFFSet LO | SIDE SAVe | INCLude | [:STATe] SPECtrum | AUTOtune STAtus | REPort?
|
Click on a red keyword to view the command details.
See Also
(Read-Write) Set and read the VNA to VSA connection state. |
|
Parameters |
|
<ch> |
Any existing SA or MOD/MODX channel. If unspecified, value is set to 1. |
<bool> |
Choose from: OFF (or 0)- Disconnect VNA from VSA 89600 ON (or 1)- Connect VNA to VSA 89600 |
Examples |
SENS:VSA:CONN ON |
Query Syntax |
SENSe<ch>:VSA:CONNect[:STATe]? |
Return Type |
Boolean |
OFF |
|
(Read-Write) Set to stream input power to a VSA measurement channel. |
|
Parameters |
|
<ch> |
Any existing SA or MOD/MODX channel. If unspecified, value is set to 1. |
<bool> |
Choose from: OFF (or 0) - Do not stream input power to VSA. ON (or 1) - Stream input power to VSA. |
Examples |
SENS:VSA:DATA:MOD:PIN1 ON |
Query Syntax |
SENSe<ch>:VSA:DATA:MOD:PIN1[:STATe]? |
Return Type |
Boolean |
ON |
|
(Read-Write) Set to stream ideal input power to VSA measurement channel. |
|
Parameters |
|
<ch> |
Any existing SA or MOD/MODX channel. If unspecified, value is set to 1. |
<bool> |
Choose from: OFF (or 0) - Do not stream ideal input power to VSA. ON (or 1) - Stream ideal input power to VSA. |
Examples |
SENS:VSA:DATA:MOD:PINWav ON |
Query Syntax |
SENSe<ch>:VSA:DATA:MOD:PIN1[:STATe]? |
Return Type |
Boolean |
ON |
|
(Read-Write) Set to stream output power to a VSA measurement channel. |
|
Parameters |
|
<ch> |
Any existing SA or MOD/MODX channel. If unspecified, value is set to 1. |
<bool> |
Choose from: OFF (or 0) - Do not stream output power to VSA. ON (or 1) - Stream output power to VSA. |
Examples |
SENS:VSA:DATA:MOD:POU2 ON |
Query Syntax |
SENSe<ch>:VSA:DATA:MOD:POU2[:STATe]? |
Return Type |
Boolean |
ON |
|
(Read-Write) Set and read the data stream state. |
|
Parameters |
|
<ch> |
Any existing SA or MOD/MODX channel. If unspecified, value is set to 1. |
<bool> |
Choose from: OFF (or 0) - Do not stream data from VNA to VSA. ON (or 1) - Stream data from VNA to VSA. |
Examples |
SENS:VSA:DATA:STR ON |
Query Syntax |
SENSe<ch>:VSA:DATA:STReam[:STATe]? |
Return Type |
Boolean |
OFF |
|
(Read-Write) Set and read the state of the digital trigger. This command is used to make the time domain IQ exported data starting time identical sweep-to-sweep. Disabling this command makes the exported data less stable from sweep-to-sweep. |
|
Parameters |
|
<ch> |
Any existing SA or MOD/MODX channel. If unspecified, value is set to 1. |
<bool> |
Choose from: OFF (or 0)- Disable digital trigger. ON (or 1)- Enable digital trigger. |
Examples |
SENS:VSA:DTR 1 |
Query Syntax |
SENSe<ch>:VSA:DTRigger[:STATe]? |
Return Type |
Boolean |
ON |
|
(Read-Write) Set and read the VSA center frequency which determines the LO frequency (LO Freq = VSA Center ± IF Offset) and the display center frequency of the VNA and VSA 89600. |
|
Parameters |
|
<ch> |
Any existing SA or MOD/MODX channel. If unspecified, value is set to 1. |
<num> |
Center frequency. Choose any number between the minimum and maximum frequency limits of the analyzer. Units are Hz. |
Examples |
SENS:VSA:FREQ:CENT 6e9 |
Query Syntax |
SENSe<ch>:VSA:FREQuency:CENTer? |
Return Type |
Numeric |
3.021e9 |
|
(Read-Write) Set and read the IF offset used for calculating the LO frequency. |
|
Parameters |
|
<ch> |
Any existing SA or MOD/MODX channel. If unspecified, value is set to 1. |
<num> |
IF offset value in Hertz. The range is 0 to 21 MHz. |
Examples |
SENS:VSA:IF:OFFS 20e6 |
Query Syntax |
SENSe<ch>:VSA:IF:OFFSet? |
Return Type |
Numeric |
21e6 |
|
(Read-Write) Set and read the LO side. |
|
Parameters |
|
<ch> |
Any existing SA or MOD/MODX channel. If unspecified, value is set to 1. |
<enum> |
Choose from: LOW - LO Freq = VSA Center - IF Offset HIGH - LO Freq = VSA Center + IF Offset |
Examples |
SENS:VSA:LO:SIDE LOW |
Query Syntax |
SENSe<ch>:VSA:LO:SIDE? |
Return Type |
Enumeration |
LOW |
|
(Read-Write) Sets to automatically save the VSA state file and embed it into the VNA state file (.csa file). |
|
Parameters |
|
<ch> |
Any existing SA or MOD/MODX channel. If unspecified, value is set to 1. |
<bool> |
Choose from: OFF (or 0)- Disable the VSA state within VNA state file ON (or 1)- Enable the VSA state within VNA state file |
Examples |
SENS:VSA:DTR 1 |
Query Syntax |
SENSe<ch>:VSA:SAVe:INCLude[:STATe]? |
Return Type |
Boolean |
ON |
|
(Write-only) Sets the VSA window in front of the VNA GUI when the VSA-to-VNA connection is running. |
|
Parameters |
|
<ch> |
Any existing SA or MOD/MODX channel. If unspecified, value is set to 1. |
Examples |
SENS:VSA:SHOW |
Not Applicable |
|
(Write-only) Sets the VSA spectrum settings to match the current SA coherent repetition rate. In addition, it forces the VSA RBW to match the coherent tone spacing. |
|
Parameters |
|
<ch> |
Any existing SA or MOD/MODX channel. If unspecified, value is set to 1. |
Examples |
SENS:VSA:SPEC:AUTO |
Not Applicable |
|
(Read-only) Reads the status of the VNA to VSA connection and configuration status. Learn more. |
|
Parameters |
|
<ch> |
Any existing SA or MOD/MODX channel. If unspecified, value is set to 1. |
Examples |
SENS:VSA:STA:REP? |
Return Type |
Char |