Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA Replaced with CALC:X? (Read-only) Returns the stimulus values for the specified channel. If the channel is sweeping the source backwards, the values will be in descending order. Note: To avoid frequency rounding errors, specify FORM:DATA <Real,64> or <ASCii, 0> |
|
Parameters |
|
<cnum> |
Any existing channel number; if unspecified, value is set to 1. |
Examples |
SENS:X? |
Return Type |
Depends on FORM:DATA command |
Not applicable |
|