Contains the settings to recorrect S11 and S22 error between the VNA and the DUT reference plane.
SYSTem:CALibrate:CALupdate AVERage | COUNt BWIDth CHANnels GATE | AUTO | STARt | COUPle | [:STATe] | STOP | COUPle | [:STATe] PORTs SETTings | AUTO SOURce | POWer
|
Click on a red keyword to view the command details.
Applicable Models: All (Write-Read) Sets and returns the averaging used to improve noise errors. |
|
Parameters |
|
<value> |
Average factor value. The default value is 1. |
Examples |
SYST:CAL:CAL:AVER:COUN 1 |
Query Syntax |
SYSTem:CALibrate:CALupdate:AVERage:COUNt? |
Return Type |
Numeric |
Default |
1 |
Applicable Models: All (Write-Read) Manually sets and returns the IF bandwidth used by the active measurement channel. Learn more. |
|
Parameters |
|
<value> |
IF bandwidth value. |
Examples |
SYST:CAL:CAL:BWID:RES 100 kHz |
Query Syntax |
SYSTem:CALibrate:CALupdate:BWIDth[:RESolution]? |
Return Type |
Numeric |
Default |
Not Applicable |
Applicable Models: All (Write-Read) Selects the channel(s) to calibrate. |
|
Parameters |
|
<value> |
Channel numbers to be calibrated. The range is 1 to 500. These channels must already exist. |
Examples |
SYST:CAL:CAL:CHAN 1,2,3 |
Query Syntax |
SYSTem:CALibrate:CALupdate:CHANnels[:SELect]? |
Return Type |
Comma separated list of channels |
Default |
Not Applicable |
Applicable Models: All (Write-Read) When set to ON, calculates the gate values automatically when the SYSTem:CALibrate:CALupdate:INITialize command is sent. As a result, user-defined Gate Start and Gate Stop values are not used and their Couple state is disabled. |
|
Parameters |
|
<bool> |
ON (or 1) - Couple all gate start times to the same value. OFF (or 0) - Do not couple all gate start times to the same value. |
Examples |
SYST:CAL:CAL:GATE:AUTO 1 |
Query Syntax |
SYSTem:CALibrate:CALupdate:GATE:AUTO? |
Return Type |
Boolean |
OFF or 0 |
|
Applicable Models: All (Write-Read) Sets and returns the gate start value for time domain gating. |
|
Parameters |
|
<value> |
Gate start time. |
Examples |
SYST:CAL:CAL:GATE:STAR -1ns |
Query Syntax |
SYSTem:CALibrate:CALupdate:GATE:STARt? |
Return Type |
Numeric |
Default |
-1ns |
Applicable Models: All (Write-Read) Sets and returns the state of gate coupling for gate start value. Enabling this function couples all gate start times to the same value set using the SYSTem:CALibrate:CALupdate:GATE:STARt command. |
|
Parameters |
|
<bool> |
ON (or 1) - Couple all gate start times to the same value. OFF (or 0) - Do not couple all gate start times to the same value. |
Examples |
SYST:CAL:CAL:GATE:STAR:COUP:STAT 1 |
Query Syntax |
SYSTem:CALibrate:CALupdate:GATE:STARt:COUPle[:STATe]? |
Return Type |
Boolean |
OFF or 0 |
|
Applicable Models: All (Write-Read) Sets and returns the gate stop value for time domain gating. |
|
Parameters |
|
<value> |
Gate stop time. |
Examples |
SYST:CAL:CAL:GATE:STop 1ns |
Query Syntax |
SYSTem:CALibrate:CALupdate:GATE:STOP? |
Return Type |
Numeric |
Default |
+1ns |
Applicable Models: All (Write-Read) Sets and returns the state of gate coupling for gate stop value. Enabling this function couples all gate stop times to the same value set using the SYSTem:CALibrate:CALupdate:GATE:STOP command. |
|
Parameters |
|
<bool> |
ON (or 1) - Couple all gate stop times to the same value. OFF (or 0) - Do not couple all gate stop times to the same value. |
Examples |
SYST:CAL:CAL:GATE:STOP:COUP:STAT 1 |
Query Syntax |
SYSTem:CALibrate:CALupdate:GATE:STOP:COUPle[:STATe]? |
Return Type |
Boolean |
OFF or 0 |
|
Applicable Models: All (Write-only) Initializes the ports selected using the SYSTem:CALibrate:CALupdate:PORTs[:SELect] command. |
|
Parameters |
|
Examples |
SYST:CAL:CAL:INIT 1,2,3 |
Query Syntax |
SYSTem:CALibrate:CALupdate:INITialize? |
Default |
Not Applicable |
Applicable Models: All (Write-Read) Selects the port numbers to initialize. |
|
Parameters |
|
<value> |
Ports numbers to be calibrated. |
Examples |
SYST:CAL:CAL:PORT 1,2,3,4 |
Query Syntax |
SYSTem:CALibrate:CALupdate:PORTs[:SELect]? |
Return Type |
Comma separated list of ports |
Default |
Not Applicable |
Applicable Models: All (Write-only) Recorrects the ports selected using the SYSTem:CALibrate:CALupdate:PORTs[:SELect] command. A port must be initialized using the SYSTem:CALibrate:CALupdate:INITialize command before it can be recorrected. |
|
Parameters |
|
Examples |
SYST:CAL:CAL:REC 1,2,3 |
Query Syntax |
SYSTem:CALibrate:CALupdate:RECorrect? |
Default |
Not Applicable |
Applicable Models: All (Write-Read) Sets and returns the reference cal set name. |
|
Parameters |
|
<calsetName> |
Cal set name. |
Examples |
SYST:CAL:CAL:REF "myCalSet" |
Query Syntax |
SYSTem:CALibrate:CALupdate:REFerence? |
Return Type |
String |
Default |
Not Applicable |
Applicable Models: All (Write-Read) Use a channel's existing IF BW, Averaging, and Power value settings or enter the values manually. |
|
Parameters |
|
<bool> |
ON (or 1) - Use a channel's existing IF BW, Averaging, and Power value settings. OFF (or 0) - Enter values for IF BW, Averaging, and Power manually. |
Examples |
SYST:CAL:CAL:SETT:AUTO 1 |
Query Syntax |
SYSTem:CALibrate:CALupdate:SETTings:AUTO? |
Return Type |
Boolean |
ON or 1 |
|
Applicable Models: All (Write-Read) Manually sets and returns the source power for the active measurement channel. |
|
Parameters |
|
<value> |
Source power value. |
Examples |
SYST:CAL:CAL:SOUR:POW -10 dBm |
Query Syntax |
SYSTem:CALibrate:CALupdate:SOURce:POWer? |
Return Type |
Numeric |
Default |
Not Applicable |