This program demonstrates the use of several External Test Set Control commands.
The SCPI commands in this example are sent over a COM interface using the SCPIStringParser object. You do NOT need a GPIB connection to run this example.
This VBScript (*.vbs) program can be run as a macro in the VNA. To do this, copy the following code into a text editor file such as Notepad and save it on the VNA hard drive as ExtTS.vbs. Learn how to setup and run the macro.
|
' Demonstrate some SCPI commands for external testsets. Dim pna Set pna = CreateObject("AgilentPNA835x.Application") Set scpi = pna.ScpiStringParser ' The K64 testset is only usable on a 4-port VNA If (pna.NumberOfPorts <> 4) Then MsgBox("This program only runs on 4-port analyzers.") Else 'If Help is active, show the measurement window and help scpi.Execute("DISP:ARR TILE") 'Return the list of supported test sets list=scpi.Execute("SENS:MULT:CATalog?") MsgBox(list) '************* K64 ***************** 'The K64 is connected using the Testset I/O 'connector. There is no handshake information. 'Therefore, a testset need not be connected. ' Load a configuration file. scpi.Execute("SENS:MULT1:TYPE 'Z5623AK64'") scpi.Execute("SENS:MULT1:ADDR 0") 'return stuff about the test set ' Returns number of input ports Inports=scpi.Execute("SENS:MULT1:INCount?") MsgBox("Input Ports: " & CStr(Inports)) ' Returns number of output ports ports=scpi.Execute("SENS:MULT1:COUNt?") MsgBox("Output Ports: " & CStr(ports)) ' Returns valid output ports for each input port For portNum = 1 To Inports ports=scpi.Execute("SENS:MULT1:PORT" & CStr(portNum) & ":CAT?") MsgBox("Port " & CStr(portNum) & " catalog: " & (ports)) Next 'Set different port mapping scpi.Execute("SENS:MULT1:ALLPorts '1 ext R,2 ext R,3 ext R,4 ext R'") 'Return port mapping portMap=scpi.Execute("SENS:MULT1:ALLPorts?") MsgBox("Ports will be mapped to " & CStr(portMap)) ' Enable external testset control and execute port mapping. This automatically enables status bar display as well. scpi.Execute("SENS:MULT1:STATe 1") MsgBox("Z5623A K64 Enabled") End If |