The following program performs either a 2-port SOLT Unknown Thru Cal or a 2-port TRL Cal. The 85052C Cal Kit used in this program contains both types of standards. This program can be run on 2-port or 4-port VNAs. When run on select PNA-L models, a Delta Match Cal is required.
This VBScript (*.vbs) program can be run as a macro in the VNA. To do this, copy the following code into a text editor file such as Notepad and save it on the VNA hard drive as Unknown.vbs. Learn how to setup and run the macro.
|
Sub PerformUnknownThruOrTRLCal() Set pna = CreateObject("AgilentPNA835x.Application") Set scpi = pna.ScpiStringParser ' Specify connectors for Ports 1 and 2 scpi.Parse "SENS:CORR:COLL:GUID:CONN:PORT1 'APC 3.5 female'" scpi.Parse "SENS:CORR:COLL:GUID:CONN:PORT2 'APC 3.5 male'" 'If your VNA has 3 or 4 ports, uncomment one or both of 'these next two lines, to explicitly specify this is a 2-port cal. 'scpi.Parse "SENS:CORR:COLL:GUID:CONN:PORT3 'Not used'" 'scpi.Parse "SENS:CORR:COLL:GUID:CONN:PORT4 'Not used'" ' Specify cal kit for Ports 1 and 2 scpi.Parse "SENS:CORR:COLL:GUID:CKIT:PORT1 '85052C'" scpi.Parse "SENS:CORR:COLL:GUID:CKIT:PORT2 '85052C'" ' Since the 85052C cal kit contains SOLT standards and also TRL ' standards, these next two lines set cal and thru method. ' Always send the init command before and after these two commands scpi.Parse "SENS:CORR:COLL:GUID:INIT" scpi.Parse "SENS:CORR:COLL:GUID:PATH:CMEThod 1,2,"SOLT" scpi.Parse "SENS:CORR:COLL:GUID:PATH:TMEThod 1,2,"Undefined Thru" ' To set up the cal as TRL, comment the previous 'CMET' line and uncomment ' this next line. The TMEThod is set by default 'scpi.Parse "SENS:CORR:COLL:GUID:PATH:CMEThod 1,2,"TRL" ' Initiate the calibration scpi.Parse "SENS:CORR:COLL:GUID:INIT" ' Query the list of ports that need delta match retStr = scpi.Parse("SENS:CORR:COLL:GUID:DMAT:APPL:PORT?") portList = Split(retStr, ",") ' If portList contains just one element and it's value is 0, then that indicates ' none of the ports being calibrated require delta match data. ' Note: if each testport on the VNA has it's own reference receiver (R channel), ' then delta match is never needed, so portList will always be just 0. lowerBound = LBound(portList) ' Delta match data is required for at least one port. ' For this example, we assume a Global Delta Match Cal has previously been ' performed so the Global Delta Match CalSet exists. ' The Global Delta Match CalSet is used when the APPL command is invoked ' without a specific calset ID (GUID). scpi.Parse "SENS:CORR:COLL:GUID:DMAT:APPL" End If ' Query the number of calibration steps retStr = scpi.Parse("SENS:CORR:COLL:GUID:STEP?") numSteps = CInt(retStr) ' Measure the cal standards For i = 1 To numSteps prompt = scpi.Parse("SENS:CORR:COLL:GUID:DESC? " & CStr(i)) retVal = MsgBox(prompt, vbOKCancel) If retVal = vbCancel Then Exit Sub retStr = scpi.Parse("SENS:CORR:COLL:GUID:ACQ STAN" & CStr(i) & ";*OPC?") Next ' Compute the error coefficients and save the cal to CalSet, and turn it on scpi.Parse "SENS:CORR:COLL:GUID:SAVE" MsgBox "Cal is done!" End Sub
|