VNA State Converter

The state file compatibility among different platforms and hardware configurations has some limitations as shown here. Especially, it is not allowed to transfer your measurement state to different platforms, such as PXI to Streamline.

VNA State Converter enables transferring your measurement states among different platforms and hardware configurations. For example, you can transfer your measurement setup from PNA 4-port model to ENA 2-port model.

 

The VNA State Converter translates the VNA settings into SCPI command sequences. Then, the command sequence can be recalled and executed on another VNA unit.

 

Supported Models

Limitation:

The state converter cannot transfer the following states.

 

How to execute VNA State Converter

Using Hardkey/SoftTab/Softkey

Using a mouse

  1. Press SaveRecall > Save Other > VNA State Converter > Converter Tool...

  1. Click Utility  > Save > VNA State Converter > Converter Tool...

The following VNA State Converter Panel is displayed.

Sample Operation

  1. Configure your measurement setup.

  2. Press SaveRecall > Save Other > VNA State Converter > Converter Tool.

  3. Click to generate the SCPI command sequence.

  4. Click  to Save the setting to the HRS (.hrs) file.

  5. Transfer the HRS (.hrs) file in the target unit..

  6. Click  to recall the state setup.

  7. Close Click  to Save the setting to the file.

(A) Menu and Tool Icon

 

Commands

Icon

Description

File

Load File...

Open the recording file with .vrec file extension

Save File...

Save the recording file with .vrec file extension.

Export Sequence...

-

Export the command sequence in a text format

Exit

-

Exit the VNA state converter application

Sequence

Record State Sequence

Capture the state sequence and create the command sequence.

Play

Play the state sequence in the list on the VNA.

Custom Sequence...

-

This allows you to add SCPI commands at the end of sequence. If identical commands are present earlier in the sequence, the settingd will be overwritten accordingly.

Load... Load a text file (.txt) into the custom sequence block.

Save... Save the commands in the custom sequence block into a text file (.txt)

Clear    Clear the custom sequence block.

(B) State Tree

Display the setup tree on each channel and common functions after click .

(C) SCPI Command Table

Command: SCPI command. When you click the command in State Tree, the corresponding command is displayed at the top of row.

Parameter: you can change the parameter value by clicking the cell. 

(D) Status Bar

Show the current status

Ready/Recording state sequence/Playing state sequence