The Default System Calibration creates a system cal for TDR, GDM, and other uses. This adjustment is for service only; not for measurement calibration.
DC ECal or Mechanical Calibration Kit
See VNA Accessories
Notes
|
Click Utility, then System, then Service, then Adjustment Routines...
At
the Adjustments selection, click System
Default Calibration. The
System Default
Calibration dialog is displayed
as shown below.

Select the calibration method (ECal or Mechanical Standards).
Click on the Begin Cal button to begin the calibration.
Follow the instructions displayed in the program.
The correction data is stored in the hard drive.