This adjustment is required when upgrading. Adjustments are made to the IF amplitude, phase, and offsets.
Note: For phase adjustment, the U9391C 10 MHz to 26.5 GHz comb generator is recommended for best results instead of the higher frequency comb generator models.
IF response adjustment is required when upgrading to Option S93090xA/B, S93093A/B, or S93094A/B. In addition, this adjustment must be performed each time a new configuration is set up or if cables are changed.
Latest firmware
For Broadband systems (Option S93093A/B):
Leave ports open
Connect a thru
For Banded systems (Option S93094A/B):
Apply a short to the waveguide ports
U9391x comb generator (phase adjustment only)
U9391-60009 sine to square wave converter (phase adjustment only)
+15 VDC power supply (phase adjustment only)
USB cables (2) (phase adjustment only)
RF cable
Adapters as needed
Click Utility, then System, then Service, then Adjustment Routines....
At the Adjustments selection, click IF Response Adjustment.

Select the desired adjustments then click Begin.
Follow the instructions displayed in the program.
The correction data is stored in the flash memory on the Test Set Mother Board.