Span

Changes the displayed frequency range symmetrically about the center frequency. While adjusting Span, Center Frequency is held constant, which means that both Start Freq and Stop Freq will change.

Pressing Span also sets the frequency entry mode to Center/Span. In Center/Span mode, the Center Frequency and Span values are displayed below the graticule, and the default active function in the Frequency menu is Center Frequency.

Span also includes a toggle switch to go back and forth between Swept Span and Zero Span. Zero Span is a special sweep type in which the instrument stops sweeping over a range of frequencies, and stays at the Center Frequency. In Zero Span, the instrument sweeps in the time domain, showing you the instantaneous amplitude versus time at the Center Frequency. For more details, see Zero Span. Selecting Swept Span places the instrument in Center/Span frequency entry mode.

When in Zero Span, you can return to your last Swept Span by pressing the Swept Span/Zero Span toggle on Span. (This replaces the Last Span function found on older HP/Agilent/Keysight Analyzers.)

NOTE

We use the term Swept Span to mean spans other than Zero Span, even though sometimes when we are in what we call a Swept Span we might be performing an FFT-style sweep, which is not a true Swept Span.

If Span is set to a value greater than the maximum allowable span of the instrument, an error message is generated indicating the data is out of range and was clipped to upper limit.

Remote Command

[:SENSe]:FREQuency:SPAN <freq>

[:SENSe]:FREQuency:SPAN?

Example

Set the span to 2 GHz:

:FREQ:SPAN 2GHz

Dependencies

If the electrical attenuator is enabled, any attempt to set Span such that the Stop Freq would be >3.6 GHz results in an error

If Source Mode is set to Tracking, and Span is therefore limited by the limits of the source, a warning message is generated, “Data out of range; clipped to source max/min” if these limits are exceeded. Note that for an external source, these limits can be affected by the settings of Source Numerator, Source Denominator, and Power Sweep

In instruments with an RF Preselector, such as MXE, you cannot sweep across the band break at 3.6 GHz while the RF Preselector is on in Continuous sweep, because there is a mechanical switch that bypasses the RF Preselector above 3.6 GHz. For details, see Stop Freq

Couplings

Span affects Res BW, Sweep Time, FFT & Sweep choice (including FFT Width, Phase Noise Optimization and ADC Dither auto couplings)

When operating in Swept Span:

  • When the value is being set through the front panel numeric keypad or the SCPI command, any value of Center Frequency or Span that is within the frequency range of the instrument is allowed. The other parameter is forced to a different value, if necessary, to keep Start Freq and Stop Freq within the instrument’s frequency range

  • When using the knob or the step up/down keys, or the UP |DOWN keywords in SCPI, the value that is being changed, that is, Center Frequency or Span, is limited so that the other parameter is not forced to a new value

Span cannot be set to zero by setting Start Freq = Stop Freq. The value of the last setting changes to maintain a minimum difference of 10 Hz between Start Freq and Stop Freq

Preset

Depends on instrument maximum frequency, mode, measurement, and selected input

See Span Presets

State Saved

Saved in instrument state

Min

10 Hz, unless entered directly, then 0 Hz is allowed, but no value between 0 and 10 is ever allowed

If the Zoomed Trace window is visible, Zero Span is not allowed, so Span may not go below 10 Hz

If the Zone Spectrum window is visible, Zero Span is not allowed in the Spectrum window, so Span may not go below 10 Hz in the Spectrum window

Max

Depends on instrument maximum frequency, mode, measurement, and selected input. See Span Presets

If the knob or step keys are being used, depends on the value of the other three interdependent parameters: Center Frequency, Start Freq, Stop Freq

Note that, if the Source Mode is set to Tracking, the effective instrument maximum Span may be limited by the source maximum frequency

Annotation

Span <value> appears on the first line of the annotation in the lower right corner of display

Status Bits/OPC dependencies

Overlapped if Signal Track is on (OPC does not return or clear until the zooming has completed for the new span)