This is an analyzer sequence parameter which determines the number of averages (N) for the acquisition.
If N is greater than 1, the analysis intervals for the acquisition are repeated N times, the acquisition period is extended to accommodate those repetitions, and the measurement results for the repeated analysis intervals are averaged from all repetitions. Repetition of analysis intervals does not require re-triggering. The acquisition is still triggered only once.
There is no dropdown list for this field; it is necessary to enter a suitable value, or accept the default value of 1.
Note: The number of averages must not be greater than 1 when the Measurements include Basic IQ Data.