This is an analyzer sequence parameter which specifies a radio band for the selected radio standard, to be used by the test set’s analyzer for the received signal during the acquisition.
Double-click in the Band field to open a dropdown list of the choices, and select the desired band from it:
The list of bands is long, and not all bands are applicable to a given standard. The table below shows the different standards, and the values appropriate to them.
| Radio Standard | Radio Band |
|---|---|
| NONE | NONE |
| GSM or EDGE | NONE, PGSM, EGSM, RGSM, DCS1800, PCS1900, GSM450, GSM480, GSM850, GSM700, TGSM810 |
| WCDMA | NONE, BANDI, BANDII, BANDIII, BANDIV, BANDV, BANDVI, BANDVII, BANDVIII, BANDIX, BANDIX, BANDX, BANDXI, BANDXII, BANDXIII, BANDXIV |
| C2K (cdma2000) or C1X (1xEV-DO) | NONE, USCELL, USPCS, JAPAN, KOREAN, NMT, IMT2K, UPPER, SECOND, PAMR400, PAMR800, IMTEXT, PCS1DOT9G, AWS, US2DOT5G, PUBLIC, LOWER |
| LTE (LTE-FDD) | NONE, BAND1, BAND2, BAND3, BAND4, BAND5, BAND6, BAND7, BAND8, BAND10, BAND11, BAND12, BAND13, BAND14, BAND17, BAND18, BAND19, BAND20, BAND21, BAND24, BAND25 |