This is an analyzer sequence parameter which is used by the test set's analyzer to determine the channel plan to be used when computing the Frequency/Channel values.
Double-clicking in the Device field opens a dropdown list of the choices: BTS (Base Transceiver Station) or MS (Mobile Station). However, only the default setting (MS) is currently supported, so this field should be left as is.