Standard

This is an analyzer sequence parameter which specifies a radio standard to be used by the test set’s analyzer for the received signal during the acquisition.

Double-click in the Standard field to open a dropdown list of the choices, and select the desired standard from it (for a fixed frequency, select NONE):

Note

"C1X" represents 1xEV-DO, "C2K" represents cdma2000, and "LTE" represents LTE-FDD.

Regardless of which standard is selected, four basic measurement results (Basic Tx Power, Basic Phase Error, Basic Freq Error, and Basic IQ data) are always available. The availability of other measurements depends upon the radio standard selected here; see Measurements for more information.