:FUNCtion:PARameters:AMPLify:GAIN

Command Syntax

:FUNCtionN:PARameters:AMPLify:GAIN <gain>

<gain> is a double.

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:AMPLify:GAIN?

Description

Specifies the gain of an Amplify math operator (:FUNCtion:FOPerator).

Example Command Sequence

:FUNCtion2:FOPerator AMPLify
:FUNCtion2:PARameters:AMPLify:GAIN 1.5
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.