:FUNCtion:PARameters:AVERage:ECOunt

Command Syntax

:FUNCtionN:PARameters:AVERage:ECOunt <count>

<count> is a int.

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:AVERage:ECOunt?

Description

Specifies the count of an Average math operator (:FUNCtion:FOPerator).

Example Command Sequence

:FUNCtion2:FOPerator AVERage
:FUNCtion2:PARameters:AVERage:ECOunt 64
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.