:FUNCtion:PARameters:DELay:TIME

Command Syntax

:FUNCtionN:PARameters:DELay:TIME<delay_time>

<delay_time> is a double.

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:DELay:TIME?

Description

Sets the time delay for a Delay operator (:FUNCtion:FOPerator).

Example Command Sequence

:FUNCtion2:FOPerator DELay
:FUNCtion2:PARameters:DELay:TIME 10.6E-12
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.