:FUNCtion:PARameters:SMOoth:POINts

Command Syntax

:FUNCtionN:PARameters:SMOoth:POINts <points>
            

<points> is a integer.

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:SMOoth:POINts?

Description

Specifies the number of smoothing points in a Smooth operator (:FUNCtion:FOPerator).

Example Command Sequence

:FUNCtion2:FOPerator SMOoth
:FUNCtion2:PARameters:SMOoth:POINts 31
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…
                  //  Your code to synchronize execution timing.