Common :STATus:REASon? Query for Statistical Measurements

Query Syntax

:STATus:REASon?

Query Response

Refer to the table "Common Reasons for INV or QUES Status".

Description

Returns a string that explains the reason for a failed common statistical measurement results. If the measurement was successful, a null string is returned. Use the :STATus? query to determine if the measurement has failed.