Image Saves with Autonumbers
Example Script
disk-screen-image-capture-autonumber.py
#!python3
"""This program illustrates saving screen images to the
Infiniium XR8 oscilloscope disk with autonumbered file
names, first using custom file names, then using standard
file names.
"""
# Import modules.
import pyvisa
import sys
# Global variables.
oscilloscope_visa_address = "TCPIP0::localhost::hislip0,4880::INSTR"
timeout = 20000 # 20 seconds.
scope_base_directory = "%USER_DATA_DIR%\\"
def exit_program():
"""Exit program."""
# Close connection to oscilloscope.
sys.stdout.write("Closing oscilloscope connection.\n")
Infiniium.write(":SYSTem:GTLocal") # Unlock GUI.
Infiniium.clear() # Clear oscilloscope communications interface.
Infiniium.close() # Close communications interface to oscilloscope.
rm.close() # Close resource manager.
print("End of program.")
sys.exit()
def check_error_queue(when):
"""Check error queue."""
errors_found = False
while True:
# Keep reading errors until "No error".
error_string = Infiniium.query(":SYSTem:ERRor:NEXT? DIAGnostic")
if error_string: # If there is an error string value.
if error_string.find("0,", 0, 2) == -1: # Not "No error".
errors_found = True
print(f"ERROR: {error_string}")
else: # "No error"
break
else: # :SYSTem:ERRor:NEXT? DIAGnostic should always return string.
errors_found = True
print("ERROR: :SYSTem:ERRor:NEXT? DIAGnostic returned nothing.")
break
if errors_found:
print(f"Exited because error(s) found when: '{when}'")
exit_program()
# ==========================================================
# Main program:
# ==========================================================
# Connect and initialize oscilloscope.
rm = pyvisa.ResourceManager("C:\\Windows\\System32\\visa64.dll")
try:
Infiniium = rm.open_resource(oscilloscope_visa_address)
except Exception:
print(
f"Unable to connect to oscilloscope at {oscilloscope_visa_address}. Aborting program."
)
sys.exit()
Infiniium.timeout = timeout # Set global timeout.
Infiniium.clear() # Clear the instrument bus.
# Lock GUI happens automatically.
# Save image files using custom names. Autonumber starting at 100.
print("Four custom filenames with autonumbers:")
filename = f"{scope_base_directory}DUT_1"
Infiniium.write(f':DISK:SIMage:FNAMe "{filename}.png"')
for i in range(1, 5):
Infiniium.query(":DISK:SIMage:SAVE;*OPC?")
print(f'Saved: {Infiniium.query(":DISK:SIMage:FNAMe?").strip()}')
Infiniium.write(":DISK:SIMage:FNAMe:AUPDate")
# Save image files using standard names and autonumber.
print("Four standard filenames with autonumbers:")
Infiniium.write(":DISK:SIMage:FNAMe:USTandard")
for i in range(1, 5):
Infiniium.query(":DISK:SIMage:SAVE;*OPC?")
print(f'Saved: {Infiniium.query(":DISK:SIMage:FNAMe?").strip()}')
Infiniium.write(":DISK:SIMage:FNAMe:AUPDate")
# Check error queue.
check_error_queue("End of program")
# Exit program.
exit_program()