There are several ways to select the measurement point.
Option 1 : At either single point measurement display or list measurement display, press Stim Prev or Stim Next key to select the desired measurement point.
At the single point measurement display, point number is shown at the top-left of the screen.
Option 2: Click on the Root Menu softkey button at the top-right of the screen. From the E4982A Root softkey menu, click on Active Point softkey and enter the desired measurement point.
Option 3: Alternatively, when you are at list measurement display, you can use the mouse to click on the desired measurement point.