Change the averaging factor of an already set measurement point by following these steps:
Enter a new averaging factor. To set the averaging factor to 10 for example, press 1 and 0 and then ×1. Optionally, click to highlight the value in the averaging factor. Then, by using mouse scroll button, scroll up or down to change the value in the cell.