In the presetting, all BINs are turned OFF (inactive), and the BIN is regarded as non-existent. This requires the BIN to be turned ON (activated) either before or after setting the BIN range to make the new settings active. You can set the condition of a specific BIN and then turn it OFF temporarily. After that you can turn it ON whenever required (the setting of the BIN range is not affected by turning the BIN ON and OFF).
The following figure shows an example where BIN 1 is turned ON.