When BIN sorting setup is completed, follow these steps to turn ON the BIN sorting function.
Click on the Comparator softkey to turn ON/OFF the BIN sorting execution (the setting toggles with each press of the key).
Softkey Label |
Display Status |
Comparator [ON] |
ON (BIN sorting is executed) |
Comparator [OFF] |
OFF (BIN sorting is not executed) |
When BIN sorting is turned ON, the BIN sorting result is displayed for each measurement in the BIN sorting result area in the lower left area of the display.
The following figure shows the BIN sort result display. In this example, the latest bin is BIN 1.
In the above figure, Latest shows the BIN number of the BIN sort result. When the measurement result is not sorted in any of the BINs, OUT is displayed. When Overload or Rdc limit deviation occurred, Invalid is displayed. When the measurement result is sorted in Good Bins defined by Setting Faulty BIN, the BIN sort result is displayed in blue; when the measurement result is sorted in Faulty Bins the BIN sort result is displayed in red.