The following procedure can be used to save the setting values and measurement result list components of the measurement point setup table, calibration kit setup table and compensation kit setup table of the E4982A on a storage device in the CSV format (.csv).
Press Data Export > Export All Setup Tables.... (or Press Stim Table > All Table > Export All Setup Tables....)
The setup table Save As dialog box is displayed.

The saved CSV-format data is a text file. This file can be opened using a text editor such as Notepad application. Figure below shows an example of the setup table data in CSV-format.

The CSV-format data can be displayed with a formatted style in a spreadsheet application. Figure below shows the CSV data displayed in Microsoft Excel.

You can recall the setting.
Press Stim Table > All Table > Import All Setup Tables....
Open dialog box is displayed.
Select the desired file.