Protecting E4982A

To protect your E4982A, follow the instructions below:

  1. Read the warning labels and specifications

Do not exceed the values provided in the specifications guide or as indicated by the yellow warning labels on the front panel of the E4982A. Refer to the specifications for the conditions required to meet the listed specifications. There will be information regarding E4982A settings, and calibration requirements.

  1. Do NOT Plug off Power Cable during Shutdown Process

Do Not Plug off Power cable until completely completing the shutdown process.

If you directly interrupt the power supply to the power cable receptacle when the power supply is ON, or turn OFF the Line Switch (Always ON), the shutdown process will not work. This could damage the storage of the E4982A.

  1. Do NOT Modify or Reconfigure the Operating System

The Microsoft Windows operating system has been modified and optimized by Keysight to improve the performance of the E4982A.

  1. Install Antivirus Protection

The E4982A does NOT have antivirus protection when shipped. Use of an antivirus program is strongly recommended if you connect the E4982A to the LAN (Internet).

In addition, the use of a firewall could help to protect the E4982A from viruses. However, some firewalls could limit DCOM connectivity of the E4982A.

  1. Install Windows Critical Updates

The E4982A is always shipped with the latest service packs and critical updates that were available at the time when Firmware is updated. We recommend that you maintain the latest available protection for your E4982A by automatically accepting and installing the latest critical security patches from the Microsoft Windows Update website: http://windowsupdate.microsoft.com

  1. Run Error Check and Disk Defragmenter

When the E4982A is shutdown unexpectedly or power is removed without first shutting down, large amounts of Hard Disk Drive space is rendered unusable. If inappropriate shutdown is performed repeatedly, the E4982A could become unstable and no longer work.

This HDD space can be recovered by first running Windows Error-checking to find and correct errors on the disk, and then the Disk Defragmenter to recover Hard Disk Drive space. See the Windows Help file for more information about Disk Defragmenter.

To run error check and defragmenter follow the procedure below:

  1. Start > My Computer.

  2. Right click on C:\ drive, then click Properties.

  3. Click the Tools tab.

Error-checking

  1. Click Check Now....

  2. Check Automatically fix file system errors.

  3. Click Start.

  4. Click Yes to run disk check on next restart.

  5. Manually restart the E4982A. The disk check will run before Windows restarts.

Periodically, check the second box in addition to the first box. The error-checking process takes much longer, but performs a complete check.

Defragmentation

  1. Click Defragment Now....

  2. Click Defragment to begin the defragment process.

  3. Click Close when defragmentation is complete.

  1. Precaution for Use of Hard Disk

Do NOT Modify or delete any Files and Folders in Drive other than D and E: Drive.(These two drives, D and E are available to use as Data backup). Doing so will result in malfunctioning of the device. It is required to execute the System recovery if there are any troubles with the above operations.

  1. Precaution for RF input connector and cable

  1. Precautions for Electrostatic Discharge (ESD)

ESD can damage or destroy electronic components. Whenever possible, conduct testing at a static-safe workstation. Keep static-generating materials at least one meter away from all components. Before connecting any coaxial cable to an analyzer, momentarily short the center and outer conductors of the cable together.

  1. Maintain working environment condition

Control your environment. Maintain temperature & humidity with a satisfactory range within the instruments specification and prevent large fluctuations.

  1. Precautions for transportation

  1. Check for Proper Ventilation

Periodically check and clean the cooling vents of the E4982A. Inadequate airflow can result in excessive operating temperatures which can lead to instrument failures. When installing the product in a cabinet, the convection into and out of the instrument must not be restricted.

See the installation guide in detail.

  1. Precautions for Proper Grounding