:CALCulate:COMParator[:STATe] {ON|OFF|1|0}
:CALCulate:COMParator[:STATe]?
Turns ON or OFF the comparator. This setting is linked with the ON/OFF status of the handler interface.
|
Parameter |
State |
|
Description |
ON/OFF the comparator |
|
Range |
Select from the following: ON or 1: Turns ON the comparator OFF or 0: Turns OFF the comparator |
|
Preset value |
OFF or 0 |
{1|0}<newline><^END>
Analysis > Comparator > {ON|OFF}