:CALCulate:COMParator:OGBins <numeric>
:CALCulate:COMParator:OGBins?
Specifies the boundary between good and bad bins (the OUT_OF_GOOD_BINS line) by specifying the number of the good bin that is adjacent to the boundary. All bin numbers that are equal to or smaller than the specified bin number indicate good bins while those larger than the specified number represent bad bins.
When a DUT is sorted into a bad bin, the handler interface output signal /OUT_OF_GOOD_BINS becomes active (Low). Also, the /OUT_OF_GOOD_BINS signal becomes active when a DUT is not sorted into any of the bins 1 through 13.
|
Parameter |
Value |
|
Description |
Number of good bin to be adjacent to the boundary |
|
Range |
1 to 13 |
|
Preset value |
10 |
|
Resolution |
1 |
If your specified parameter is beyond the valid range, the instrument ignores the parameter and uses either the maximum or minimum value depending on whether the parameter is greater than the upper limit or smaller than the lower limit.
{numeric}<newline><^END>
Stim Table > Comparator tab > Rdc Limit > Good Bins drop-down menu, or
Analysis > Edit Comptr Table > Rdc Limit > Good Bins drop-down menu