:CALCulate[:MATH]:EXAMine[:MEMory]:SIZE <numeric>
:CALCulate[:MATH]:EXAMine[:MEMory]:SIZE?
Sets the maximum number of measurement data logged in the volatile memory for statistical analysis. The maximum number must be set as Param × Nop × Times where:
|
Param |
Number of displayed measurement items covering measurement parameters 1 through 4, test signal current/voltage level and Rdc. |
|
Nop |
Number of measurement points in one measurement (that is, 1 during single-point measurement or the number of measurement points in the active table during list measurement). |
|
Times |
Number of measurements needed for statistical analysis. |
|
Parameter |
Value |
|
Description |
Maximum number of measurement data |
|
Range |
1 to 1,000,000,000 |
|
Preset value |
3000 |
|
Resolution |
Obtained data number at one measurement (Param×Nop) |
If your specified parameter is beyond the valid range, the instrument ignores the parameter and uses either the maximum or minimum value depending on whether the parameter is greater than the upper limit or smaller than the lower limit.
If your specified parameter is not a multiple of (Param×Nop), the instrument ignores the parameter and uses the next highest acceptable value above the specified parameter.
{numeric}<newline><^END>
Analysis > Log size > <numeric>