:CALCulate:UFORmat{1-4}:UNIT <String>
:CALCulate:UFORmat{1-4}:UNIT?
Specifies the unit of user parameter.
|
Parameter |
String |
|
Description |
Define the unit of user parameter up to four letters or characters. To display the special character such as Ω (ohm) you can use unicode character. \uXXXX represents a UNICODE character. The unicode of Ω is "u\2126". µ is "u\00B5". |
|
Preset value |
Parameter 1: "dB" parameter 2: "deg" parameter 3: "A" parameter 4: "V" |
{string}<newline><^END>
Prmtr > Define User Formats > Unit