:DATA[:DATA]:VMON?
Returns the result of monitoring the voltage level of the test signal. If the measurement fails because of overload, the command returns 9.9E37. (Query only)
|
Parameter |
Array of Real |
|
Description |
For single-point measurement {numeric}<newline><^END> The command returns the monitored value (real number) of the measured point. For list measurement {numeric 1},...,{numeric N}<newline><^END> |
The command returns the monitored value (real number) at each point defined in the active table. Therefore, the returned data contains as many monitored values as the number of measurement points (N) and is sent in the order of measurement point numbers.
No equivalent keys are available on the front panel.