:DISPlay:BACKlight {ON|OFF|1|0}
:DISPlay:BACKlight?
Turns ON or OFF the backlight of the LCD screen. If the backlight is OFF, you cannot read information displayed on the screen.
|
Parameter |
State |
|
Description |
Turns ON/OFF the backlight of the LCD screen. |
|
Range |
Select from the following: ON or 1:Turns ON backlight. OFF or 0: Turns OFF backlight. |
|
Preset value |
ON or 1 |
{1|0}<newline><^END>
System > Service > Back Light > {ON|OFF}