:DISPlay:UPDate {ON|OFF|1|0}
:DISPlay:UPDate?
This command sets periodic updates of the LCD to ON or OFF. When periodic updates is set to ON, measurement values are updated periodically even if the measurement time is long. When periodic updates is set to OFF, measurement values are updated only when the last point in the table is measured.
|
Parameter |
State |
|
Description |
Dummy Parameter |
|
Range |
ON or 1 - Sets the periodic updates to ON OFF or 0 - Sets the periodic updates to OFF |
|
Preset value |
ON or 1 |
<state><^END>
System > Misc Setup > Periodic Update