*LRN?
This command gets the device setup query. This command is defined as "Learn Device Setup Query" in IEEE 488.2. The command returns instrument settings by binary block data (same as Save/Recall state file contents) with "SYSTem:SET " prefix.
Dim LRNData() As Byte, SETData() As Byte, NoofByte As Double
'*** Get the LRN data as Binaray data
Age4982.WriteString "*LRN?", True
LRNData = Age4982.ReadIEEEBlock(BinaryType_UI1, False, True)
'*** Save the LRN data in the file
Open "C:\LRN.dat" For Binary As #1
Put #1, , LRNData()
Close
MsgBox "Get Data"
'*** Recall the LRN data from the file
Open "C:\LRN.dat" For Binary As #1
NoofByte = LOF(1)
ReDim SETData(NoofByte)
Get #1, , SETData()
Close
'*** Send the LRN data to E4982A
Age4982.IO.Write SETData, NoofByte
<binary><newline><^END>
No equivalent key is available on the front panel.