*OPC
*OPC?
This command sets/gets the OPC bit (bit 0) in the Standard Event Status register when all pending operations are completed.
When this is used as query, 1 is returned when all pending operations are complete
{1}<newline><^END>
No equivalent key is available on the front panel.