:LXI:IDENtify[:STATe] {ON|OFF|1|0}
:LXI:IDENtify[:STATe]?
This command changes the state of the LXI status indicator.
|
Description |
State of the LXI status indicator |
|
Range |
ON or 1: Sets the LXI Status Indicator to the "IDENTIFY" state. OFF or 0:Sets the LXI Status Indicator to the "NORMAL" state. |
|
Preset value |
OFF or 0 |
{1|0}<newline><^END>
No equivalent keys are available on the front panel.