:MMEMory:COPY <string 1>,<string 2>
This command copies a file.
To specify the file, use a file name accompanying an extension. If you want to specify a file residing on the floppy disk, you must attach "A:" to the head of the file name. To use the directory and file names for specification, separate them using a slash (/).
If the specified source file is not found, an error will occur and the command will be ignored. Note that, if the file that has the same name as the specified source file already exists, it will be overwritten. (No query)
|
Parameter |
<string 1> |
<string 2> |
|
Description |
Source file name |
Destination file name |
|
Data type |
String |
String |
|
Range |
Up to 248 characters (including extension) |
Up to 248 characters (including extension) |
Save/Recall > File Utility...