:MMEMory:DELete <string>
This command deletes an existing file or directory (folder).
If a directory is specified, all files and directories in it will be deleted.
To specify a file, use a file name accompanying an extension. To specify a file (directory) under an existing directory, use a slash (/) to separate directory names or a directory and a file (or directory) name.
If you specify "D:/USER" for the directory name, all user-created files and directories in the E4982A built-in storage will be deleted.
If the specified file or directory is not found, an error will occur and the command will be ignored. (No query)
|
Parameter |
<string> |
|
Description |
Deletes an existing file or directory |
|
Data type |
String |
|
Range |
Up to 248 characters (including extension) |
Save/Recall > File Utility...