:MMEMory:LOAD <filename>, [csv_type]
Recalls the instrument settings from the file previously saved with the :MMEM:STOR command.
You can recall the file whose extension is *.sta or *.csv (setup table or bin table only).
You must specify the file name with the extension. When you specify a file under a directory, delimit the directory and file names with a slash (/).
If your specified file is not found, the command fails and an error is generated.
|
Parameter |
<filename> |
<csv_type> |
|
Description |
Name of file to recall |
You should specify the second parameter only if the file extension is ".csv". When this parameter is not specified for any file with the extension ".csv", SETup will be used. |
|
Data type |
String |
Enumerator |
|
Range |
- |
SETup: Specifies that contents of all measurement point setup tables, contents of all calibration kit setup tables, and contents of all compensation kit setup tables are recalled. COMParator: Specifies that contents of all BIN sorting setup tables are recalled. |
|
Length |
Up to 248 characters (including extension) |
Up to 248 characters (including extension) |
Save/Recall > Recall State