:MMEM:TRAN

Syntax

:MMEMory:TRANsfer <file_name>, <data>

:MMEMory:TRANsfer? <file_name>

Description

This command sets/returns data to/from a file on the built-in storage device.

Variable

Parameter

<file_name>

Description

File name on the built-in storage device

Data type

String

Range

Up to 248 characters

 

Parameter

<data>

Description

Data written on/read out from the file

Data type

Block

Query Response

{block}<newline><^END>

Equivalent key

No equivalent keys are available on the front panel.