:SERV:PROG:EXEC

Syntax

SERVice:PROGram:EXECute <file_name>, [<params>]

Description

This command executes the specified program on windows.

Variable

Parameter

<file_name>

Description

Program or file name to be executed.

If the specified file is not executable, a program associated with its extension opens the file

Data type

String

Range

Up to 255 characters

 

Parameter

<data>

Description

Parameter list. This is option.

Data type

String

Range

Up to 255 characters

Equivalent key

No equivalent keys are available on the front panel.